The N7624B Signal Studio for LTE/LTE-Advanced FDD software enables you to load Library Waveforms from the following waveform types that you can use to evaluate Multi-Standard Radio (MSR) effects on LTE signals:
N7600B Signal Studio for W-CDMA/HSPA+
N7601B Signal Studio for cdma2000/1xEV-DO
N7602B Signal Studio for GSM/EDGE/Evo
N7612B Signal Studio for TD-SCDMA/HSDPA
N7617B Signal Studio for WLAN
N7624B Signal Studio for LTE/LTE-Advanced FDD (non-MSR waveforms)
N7625B Signal Studio for LTE/LTE-Advanced TDD (non-MSR waveforms)
In the figure below, an Library Waveform is selected for configuration. Refer to MSR - Generating a Library Waveform.
|
Carrier n -- Library Waveform |
|---|
MSR - Generating a Library Waveform
MSR - Using the Library Waveform Manager
Overcoming Test Challenges of MSR Base Station Components and Transmitters